Undefined function 'ert_make_rtw_hook' for input arguments of type 'struct'.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Undefined function 'ert_make_rtw_hook' for input arguments of type 'struct'.

2,131 Views
EdnaFenner
Contributor I

I've been trying to run an example from NXP_MBDToolbox_S32K1xx toolbox using simulink, but getting an error while building the model. I have attached the screenshot of the error for the reference. Please help me with the same.

0 Kudos
Reply
2 Replies

2,068 Views
leonggz
Contributor II

seems like you don't have the license. 

type: >> ver

on the matlab prompt. you would need matlab coder and simulink coder to proceed with these code gen examples

0 Kudos
Reply

2,121 Views
SorinIBancila
NXP Employee
NXP Employee

Hello EdnaFenner,

In order to identify the problem and a possible solution, can you provide some extra information? 

What Matlab Version did you use? What version of the toolbox did you install? Can you provide steps to replicate the problem?

Best regards,

Bancila Sorin

0 Kudos
Reply