Unable to use Blocking mode in FCAN_Receive block(Model-Based Design Toolbox for MPC57xx, Version 3.0.0)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to use Blocking mode in FCAN_Receive block(Model-Based Design Toolbox for MPC57xx, Version 3.0.0)

6,398件の閲覧回数
littlepirate
Contributor I

Hi,

   I can use the CAN_Receive_Data_Trigger module in model-based Design Toolbox for MPC57xx, version 2.0.0, but I cannot use it in version 3.0.0.

   With this Error: simulink. DataType object 'status_t' is not in scope from 'untitled/FCAN_Receive'.

   Is there any good solution?

   Thank you very much!

0 件の賞賛
返信
5 返答(返信)

6,144件の閲覧回数
dea
Contributor I

Hello! I have the same problem. How did you solve this problem?

0 件の賞賛
返信

6,144件の閲覧回数
chenli2
Contributor II

No solution. No answer from NXP.

Sent from Ding Mail

0 件の賞賛
返信

6,144件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello 欣澍 杨,

The toolboxes 3.0.0 and 2.0.0 are not compatible between them, so please do not use blocks from the 2.0.0 in 3.0.0 or reverse. The MPC57xx 3.0.0 is based on S32 SDK for Power Architecture so more or less the output for some blocks are now provided from others. We also do provide examples for CAN so please have a look on them before.

Hope this helps,

Marius

0 件の賞賛
返信

6,086件の閲覧回数
j_wale_3
Contributor II

It seems this still has not been fixed in MBDToolbox version 3.2.0. Any comment from NXP, please? It's preventing commercial work in my case.

Thanks,

John.

0 件の賞賛
返信

6,144件の閲覧回数
chenli2
Contributor II

Hello,

There is NO example of CAN receive for Blocking mode. All example are non-blocking mode.  I am using Version 3.0. When I change the mode, I got error message "Simulink.DataType object 'status_t' is not in scope from 'SoftwarePlatformMPC5744/Subsystem7/CAN/CAN 0 Rx/FCAN_Receive1'.

Can you show me an example of blocking mode CAN receiver?

Li