Try to flash our own algorithm to s32k144EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Try to flash our own algorithm to s32k144EVB

5,098 次查看
shukla007
Contributor II

In image1 I am try to flash our BMS algorithm but its show error I take the reference Nxp BMS example that is in image 2 can you help me how i can flash our bms algorithm

To flash our algorithm what change required to my algorithm can you tell me

0 项奖励
回复
2 回复数

5,076 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @shukla007,

The level of detail regarding the errors you are facing you have provided in this post is too low so we could suggest any solution for your encountered issue. From the screenshot, I can see that Simulink has detected a couple of issues. My suggestion is to press on the "View 60 errors" button, and try to address each of the mentioned errors.  A possible cause is that the output data type from the BCC Get_Values block might be mismatched with the inputs of your algorithm.

mariuslucianand_0-1698068461942.png

Hope this helps,

Marius

 

0 项奖励
回复

5,047 次查看
shukla007
Contributor II

As you give the above solution I am able to solve error but I am unable to solve one error can you help me to solve that error so I can genrate the code and flash it into the s32k144 board I put a screenshot of that error 

标记 (1)
0 项奖励
回复