Software from NXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software from NXP

3,413 Views
aniket_bagade
Contributor III

dumitru-daniel.popa‌

 I have purchased MTRDEVKSPNK144 from NXP for Rapid prototyping of my control algorithm. I just wants to ask

1) weather all software tool like freemaster,MCAT and Model based design toolboxare are free of charge?

2)  is there any expiry date of License agreement of this software (freemaster)?

3 Replies

3,240 Views
Daniel_Popa
NXP Employee
NXP Employee

Yes, all the software you have mentioned above is free of charges. There is no time limit in using these software.

Best regards,
Daniel

3,240 Views
aniket_bagade
Contributor III

while installing freemaster after entering software activation code, it is asking for activation type, in both online and offline activation I am getting following error. in offline activation mode it is asking for .xtml file. can you please help me this regard.

freemaster error.PNG

0 Kudos
Reply

3,240 Views
iulian_stan
NXP Employee
NXP Employee

Hi Aniket,

 

Do you have administrative rights to run FreeMASTER installer ? (looks like it fails to install the licensing service).

Please note that only FreeMASTER Lite requires activation, you can start by using FreeMASTER (the main tool) by deselecting the FreeMASTER Lite option during component selection.

For more details check this article - FreeMASTER Installation.

Kind regards,

Iulian