Simulink external mode for S32V234

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simulink external mode for S32V234

4,068件の閲覧回数
283230333
Contributor III

The chip used by our controller is S32V234, which uses the Linux operating system. Our customers use matlab Simulink to develop our controller applications. Simulink has an external mode that can be connected to the target hardware and simulated. So we would like to ask, does S32V234 have an example that supports simulink external mode? How to support the external mode of simulink?

0 件の賞賛
返信
2 返答(返信)

3,889件の閲覧回数
paulvlase
NXP Employee
NXP Employee

Hi [email protected]‌,

Do you intend to run your applications on cortex-A53 core, in linux or standalone? Or on cortex-M4 core?

0 件の賞賛
返信

3,889件の閲覧回数
283230333
Contributor III

We want to run application on cortex-A53 core,in linux.

0 件の賞賛
返信