Simulink external mode for S32V234

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Simulink external mode for S32V234

2,979 次查看
283230333
Contributor III

The chip used by our controller is S32V234, which uses the Linux operating system. Our customers use matlab Simulink to develop our controller applications. Simulink has an external mode that can be connected to the target hardware and simulated. So we would like to ask, does S32V234 have an example that supports simulink external mode? How to support the external mode of simulink?

0 项奖励
回复
2 回复数

2,800 次查看
paulvlase
NXP Employee
NXP Employee

Hi 283230333@qq.com‌,

Do you intend to run your applications on cortex-A53 core, in linux or standalone? Or on cortex-M4 core?

0 项奖励
回复

2,800 次查看
283230333
Contributor III

We want to run application on cortex-A53 core,in linux.

0 项奖励
回复