Simulator for S32k14x devices.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simulator for S32k14x devices.

6,604件の閲覧回数
rajuparammal
Contributor I

Is there any command line simulator available for S32K14x controllers, like sim30 for PIC.

I just want to configure ceedling to run the test on the simulator.

0 件の賞賛
返信
4 返答(返信)

6,301件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi rajuparammal‌,

As far as i know NXP does not have a simulator for the S32K14x product families capable to simulate the core and peripherals.

Nonetheless, if you wish to test some generic C code on an ARM core similar with the one used by S32K14x controllers then i would suggest to look at IAR Workbench IDE. They support various ARM core simulators and depending on the code size of your project you might be able to use it for free.

Hope it helps!

Daniel 

0 件の賞賛
返信

6,303件の閲覧回数
rajuparammal
Contributor I

Hi

Thanks. I have no plans to go with IAR Workbench. Is there any good open source simulator for arm Cortex M4?

0 件の賞賛
返信

6,303件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi rajuparammal‌,

Perhaps you can have a look at QEMU: The GNU MCU Eclipse QEMU 

Based on their release notes you should expect some limitations but it should cover for most of what you wish for.

Limitations

  • QEMU accurately emulates Cortex-M3 and M4 thumb instructions; specific Cortex-M4 floating point instructions are not supported;
  • the current implementation of NVIC uses some related interrupt controller code from larger cores, and is not very accurate.
0 件の賞賛
返信

6,303件の閲覧回数
bjrajendra
Senior Contributor I

Hi Daniel,

Nice to know about the QEMU.

I actually had RAM issues & would like to replicate the same on QEMU. 

Kindly confirm whether QEMU supports RAM simulator as well.

Thanks in advance,

Raju.

0 件の賞賛
返信