Sensorless ACIM Field-Oriented Control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensorless ACIM Field-Oriented Control

3,126 Views
terre1
Contributor I

Why are there no important modules in the Model-Based Design Toolbox (MATLAB) for MCUs Kinetis KV or MPC57xx? 
  Such as: 
1. ACIM rotor flux observer. 
2. MRAS Speed Estimater. 
3. Flux weakening. 
I want to develop software for Sensorless ACIM Field-Oriented Control.

Labels (1)
0 Kudos
Reply
2 Replies

2,997 Views
terre1
Contributor I

Thanks for the answer.

0 Kudos
Reply

2,997 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi [email protected]‌,

The MBDT Toolbox supports NXP Automotive Math And Motor Control Library. 

The AMMCLIB do contains some of the functionalities you are referring too (especially the one for MPC57xx)

Anyhow, you can build your algorithms for ACIM control with standard Simulink blocks, and then use it to generate the code and deploy it to the target. It might not be as easy of using dedicated AMMCLIB, but it should work for your case.

Hope this helps!

Daniel

0 Kudos
Reply