Sample code on EKF prediction for Adaptive Battery Modelling?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sample code on EKF prediction for Adaptive Battery Modelling?

3,964 次查看
marcuslim
NXP Employee
NXP Employee

Hi,

Customer is checking if we have any jump start Matlab code for this.

They are using S32K1x and MC33771B in their new setup.

They like to run adaptive battery modelling in this new board to improve accuracy of SoC by EKF prediction in real-time, thus checking for any example code.

Regards,

Marcus

标签 (1)
标记 (3)
4 回复数

3,755 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌, marcuslim‌,

I have updated the document on https://community.nxp.com/docs/DOC-345880  by adding the Simulink example for the demo. You find all the instructions there.

Hope this helps,

Marius

3,755 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello marcuslim‌,

Nice to hear that our customer has an interest in implementing Battery Management System using our Model Based Design Toolbox for S32K in Matlab/Simulink!

Yes, we do have a starting point for this kind of application. This article How to use your own C code in our Toolbox (Battery Management System example)  presents a way of achieving converted values from MC33772B Battery controller on S32K144, in Simulink by using custom code. 

Even if the article shows the steps for the MC33772B and our customer is interested in MC33771B, NXP provides the  Embedded SW: MC33771/MC33772 SW Driver | NXP  driver, which also covers the part that our customer needs. The steps in achieving data from BMS chip, following the article, are almost identical.

Hope this helps,

Marius

0 项奖励
回复

3,755 次查看
shivamshankarg
Contributor III

Hello Marius,

can we get the sample c code written S32 Design Studio for Battery Management Systems, it would help alot as i am also going to work on battery managament system using S32K146 MCU and other peripherals i just want a demo code, so i can learn some logic. mariuslucianandrei 

0 项奖励
回复

3,755 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

You can download the driver together with the S32DS example from here Embedded SW: MC33771/MC33772 SW Driver | NXP  

Hope this helps,

Marius