SPI Initializes four chip select pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPI Initializes four chip select pins

跳至解决方案
1,959 次查看
fernando_barrio
Contributor III

Hi,

I am working with SPI on the S32K, is there any way that I don't have to initialize all four chip select pins? I want three instances of SPI communication each with only one slave/master, but now I have a lot of pins that I cannot use. Please let me know if you have any suggestions.

Thank you,

Fernando

1 解答
1,815 次查看
constantinrazva
NXP Employee
NXP Employee

Hello fernando.barrios@uwaterloo.ca‌,

I've updated this hotfix (#2) so you can select None on the pins you don't need to use. Please follow the instructions there and let me know if you encounter any issues.

Kind regards,

Razvan.

在原帖中查看解决方案

4 回复数
1,815 次查看
constantinrazva
NXP Employee
NXP Employee

Hello fernando.barrios@uwaterloo.ca‌,

In the current version of the toolbox there is no such option, but I will post on the Hotfixes page next week an update so you can do just that - it will be there probably Tuesday; I'll post here a link to it as it is made available.

Kind regards,

Razvan.

1,815 次查看
fernando_barrio
Contributor III

Hi constantinrazvan.chivu‌,

That sounds great, thank you for the support.

Fernando

0 项奖励
回复
1,816 次查看
constantinrazva
NXP Employee
NXP Employee

Hello fernando.barrios@uwaterloo.ca‌,

I've updated this hotfix (#2) so you can select None on the pins you don't need to use. Please follow the instructions there and let me know if you encounter any issues.

Kind regards,

Razvan.

1,815 次查看
fernando_barrio
Contributor III

Hi constantinrazvan.chivu‌,

Looks great, I really appreciate the help.

Thank you,

Fernando

0 项奖励
回复