SPI Initializes four chip select pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Initializes four chip select pins

Jump to solution
2,810 Views
fernando_barrio
Contributor III

Hi,

I am working with SPI on the S32K, is there any way that I don't have to initialize all four chip select pins? I want three instances of SPI communication each with only one slave/master, but now I have a lot of pins that I cannot use. Please let me know if you have any suggestions.

Thank you,

Fernando

1 Solution
2,666 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

I've updated this hotfix (#2) so you can select None on the pins you don't need to use. Please follow the instructions there and let me know if you encounter any issues.

Kind regards,

Razvan.

View solution in original post

4 Replies
2,666 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

In the current version of the toolbox there is no such option, but I will post on the Hotfixes page next week an update so you can do just that - it will be there probably Tuesday; I'll post here a link to it as it is made available.

Kind regards,

Razvan.

2,666 Views
fernando_barrio
Contributor III

Hi constantinrazvan.chivu‌,

That sounds great, thank you for the support.

Fernando

0 Kudos
Reply
2,667 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

I've updated this hotfix (#2) so you can select None on the pins you don't need to use. Please follow the instructions there and let me know if you encounter any issues.

Kind regards,

Razvan.

2,666 Views
fernando_barrio
Contributor III

Hi constantinrazvan.chivu‌,

Looks great, I really appreciate the help.

Thank you,

Fernando

0 Kudos
Reply