S32k3:Dynamic Timer on MBDT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k3:Dynamic Timer on MBDT

2,858 Views
avinashstarkenn
Contributor III

Hello,

I am using S32k344 with MBDT.

I want Timer to use ticks value defined externally.

avinashstarkenn_0-1701784845970.pngavinashstarkenn_0-1701784845970.png

I want to give ticks value as input to the block using MATLAB's 'Data Memory Write' / 'Constant' or any other write blocks.

Any other block or methods is also appreciated.

Regards

 

 

#Timer #MBDT #S32k3 #S32k344 #Simulink #Matlab

0 Kudos
Reply
6 Replies

2,830 Views
avinashstarkenn
Contributor III

Hello,

Can I know the status?

 

0 Kudos
Reply

2,821 Views
georgevictor
NXP Employee
NXP Employee

Hi, @avinashstarkenn,

We acknowledge your request to integrate the functionality of configuring timer values from an external data store memory within the GPT block. We are pleased to inform you that this requested feature will be incorporated into our upcoming Model-Based Design Toolbox (MBDT) for S32K3xx release.

Best regards,

Victor

0 Kudos
Reply

2,755 Views
avinashstarkenn
Contributor III

Status?

0 Kudos
Reply

2,816 Views
avinashstarkenn
Contributor III

Hello @georgevictor 

When will the new release be coming out.

How to integrate new release with existing MBDT for S32K3xx?

0 Kudos
Reply

2,747 Views
georgevictor
NXP Employee
NXP Employee

Hi, @avinashstarkenn,

 

The new Model-Based Design Toolbox (MBDT) for S32K3xx release is going to be launched in the second quarter of 2024. 

In order to incorporate your ongoing projects into a future release, it is generally required to migrate the configuration projects associated with the Simulink models, either EBT or S32CT. Our toolbox features an integrated migration mechanism at the model opening designed to help users in this process.

Best regards, 

Victor

 

 

0 Kudos
Reply

2,769 Views
avinashstarkenn
Contributor III

Reply/Status:

By when can we  get new mbdt release for S32k3xx.

How to integrate new release with old Mbdt?

0 Kudos
Reply