S32K3xx mbdt Documents Clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3xx mbdt Documents Clarification

2,181 Views
Wei_H
Contributor III

Hi,

I am using S32k3 mbdt in Simulink and wanted to detect bus error for CAN. 

Wei_H_0-1726783973629.png

What I want to learn more about is the state and status, which I have a hard time finding the exact documentation on these output parameter.

First, I went through documentation on the block in Mathwork. However, the html web page does not expand further when I click on it. So not enough information to answer my questions.

/static/help/3ptoolbox/nxpmodelbaseddesigntoolboxfors32k3xxseriestoolbox/doc/deployment.html

Wei_H_1-1726784294770.png

I have tried reading S32K3XXRM: S32K3xx Reference Manual to find detail about error state, but couldn't find descriptions that describes the state value that I'm observing.

Please help finding the document information about this block, thanks!

Tags (3)
0 Kudos
Reply
4 Replies

2,138 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

from HW point of view, for error detection/reporting, check chapters 73.6.2.8 Error Counter (ECR) and 73.6.2.9 Error and Status 1 (ESR1) of the S32K3xx Reference Manual.

BR, Petr

0 Kudos
Reply

2,117 Views
Wei_H
Contributor III

I do see that the manual have the section that describe ECR and ESR1. However, how am I sure that it is correlate with the blocks that I'm using in the NXP library. Since the output state can go 0, 1, or 2 base on observation, which doesn't match the section I'm looking at in the reference manual.

Another question I would like to ask is how to correlate each API function of in NXP library mbdt to the reference manual?

Thanks

0 Kudos
Reply

1,987 Views
SuperBeginner
Contributor III

Dear @PetrS ,

I also have the same question on how to correlate each API function of in NXP library mbdt to the reference manual. 

The output status of the NXP block can go 0, 1 or 2, but this also does not match the status message I looked at in the reference manual.

Could you help me, please ?

 

Thanks

0 Kudos
Reply

2,172 Views
Wei_H
Contributor III

Hi, @robertv 

 

Please take a look on this questions, thanks!

0 Kudos
Reply