S32K358-Q172 CAN transmission failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K358-Q172 CAN transmission failed

1,500 Views
XH
Contributor I

Dear @Adrian_Gherca ,

 

I hope you are well. I have built a MBDT Can transmit model mimicking the Can Transmit 342 S32CT example model in the Simulink library. However, when I observe it in Freemaster, the status of the Can_Write module is 2, which means the buffer is full or busy. ( pleas see the attached image). I have also attached the file of my whole model. Could you please help me to see where the issue is? Many thanks, Xiaomei

0 Kudos
Reply
1 Reply

1,496 Views
XH
Contributor I

Hi @Adrian_Gherca ,

 

Forgot to mention that the Can I am using is FlexCAN 6. Many thanks, Xiaomei

 

 

0 Kudos
Reply