S32K344 PIL timeout error while receiving data from the rtiostream interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K344 PIL timeout error while receiving data from the rtiostream interface

1,166 次查看
sh_dhanasekaran
Contributor II

Hi, 

I work with MATLAB 2022b and on target board S32K344-Q257. I have been trying to run the Simple PiL s32ct. 

Even though I get a message that 'the executable file has been downloaded to S32K344'

I end up with the following error!

The timeout of 10 seconds for receiving data from the rtiostream interface has been exceeded. There might be multiple reasons for this failure.
You should:

a) Check that the target hardware configuration is correct

b) Confirm that the target is running

c) Consider the possibility of application run-time failure, consider using SiL, which supports signal handlers and debugging

If you cannot find a solution, consider using the method setTimeoutRecvSecs of rtw.connectivity.RtIOStreamHostCommunicator to increase the timeout value.

0 项奖励
回复
0 回复数