S32K344 Model-Based Design Toolbox - FreeRTOS Compilation Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 Model-Based Design Toolbox - FreeRTOS Compilation Error

632 Views
Baris
Contributor II

Hello,
I am currently developing a project using the S32K344 microcontroller. When I try to integrate FreeRTOS into my model, I encounter a series of compilation errors stating that the FreeRTOS.h file cannot be found.The current versions of the toolboxes installed on my system are as follows:

Model-Based Design Toolbox for BMS Series: v1.1.0
Model-Based Design Toolbox for S32K3xx Series: v1.4.2

The BMS Toolbox version I am using is only compatible with this specific version of the S32K3xx Toolbox. Therefore, upgrading the S32K3xx toolbox is not an option for me, as it would break the BMS toolbox support. How can I manually resolve this path or dependency issue to include FreeRTOS successfully while keeping my current toolbox versions? Any guidance would be highly appreciated.

@mariuslucianand 

0 Kudos
Reply
1 Reply

577 Views
SorinIBancila
NXP Employee
NXP Employee

Hello,

Unfortunately FreeRTOS is not compatible with the specified software stack. One alternative is to export the application into S32DS and to integrate FreeRTOS from the IDE.

Best regards,

Sorin Bancila

0 Kudos
Reply