S32K3 Matlab

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 Matlab

1,694 Views
Jon123
Contributor II

Jon123_0-1747707408742.png

Hello, I'd like to ask why the error is reported to the library here. At present, I have installed the MBD package of S32K3. Open the routine inside, click Compile, Deploy and Start in the red box, and the error will be reported. Moreover, this is a library file, and I can't modify it yet. Thank you. I also took a screenshot of the reported error below.

 

0 Kudos
Reply
2 Replies

1,617 Views
AndewC2000
Contributor I

Can someone follow up about this topic,blank.png because I had similar question. Thank you appreciate for any answer..

0 Kudos
Reply

1,602 Views
Jon123
Contributor II

If you solve this problem, can you share it with me? Thank you.

0 Kudos
Reply