S32K3 MBD - MCU Support Missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 MBD - MCU Support Missing

ソリューションへジャンプ
2,020件の閲覧回数
abhishekkumarbwi
Contributor I

Dear NxP Team, 

I am using S32K312-LQFP 100 MCU. 

I am not able to find it in the Hardware Selection Tab. 

How can I find it? 

Toolbox version [Model-Based Design Toolbox for S32K3xx Series Version 1.4.0 (R2021a-R2023a)]

abhishekkumarbwi_0-1708342467139.png

 

0 件の賞賛
返信
1 解決策
1,997件の閲覧回数
georgevictor
NXP Employee
NXP Employee

Hi, @abhishekkumarbwi,

The Model-Based Design toolbox for S32K3xx includes support for the S32K12 MCU. The S32K312 MCU is available in two different packages, Q172 and Q100. Our toolbox is delivered with a default
configuration project on both EBTresos and S32 Configuration Tool only for the Q172 package. For your project, select the S32K312-Q172 Hardware Part from the model's settings, open the
configuration project that has been associated with the model and change the processor package to Q100.
Check out a similar thread that contains a more comprehensive response to your question:
MBDT 1.3.0 support for S32K312 in 100 pin MaxQFP?


Best regards,
Victor

元の投稿で解決策を見る

1 返信
1,998件の閲覧回数
georgevictor
NXP Employee
NXP Employee

Hi, @abhishekkumarbwi,

The Model-Based Design toolbox for S32K3xx includes support for the S32K12 MCU. The S32K312 MCU is available in two different packages, Q172 and Q100. Our toolbox is delivered with a default
configuration project on both EBTresos and S32 Configuration Tool only for the Q172 package. For your project, select the S32K312-Q172 Hardware Part from the model's settings, open the
configuration project that has been associated with the model and change the processor package to Q100.
Check out a similar thread that contains a more comprehensive response to your question:
MBDT 1.3.0 support for S32K312 in 100 pin MaxQFP?


Best regards,
Victor