S32K1xx MATLAB TOOL BOX installation issue: index exceeds array bonds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1xx MATLAB TOOL BOX installation issue: index exceeds array bonds

Jump to solution
4,047 Views
premch2301
Contributor III

at the last step of verify MBT license: this error is showing that index exceeds array bonds

0 Kudos
Reply
1 Solution
3,908 Views
SorinIBancila
NXP Employee
NXP Employee
Hello,

I've sent you a private message. Please check it out.

Best regards,
Sorin Bancila

View solution in original post

0 Kudos
Reply
8 Replies
3,929 Views
premch2301
Contributor III

premch2301_0-1743751063393.png

see i think there is some issue with the license file only

0 Kudos
Reply
4,029 Views
premch2301
Contributor III

premch2301_0-1743665480819.png

facing the same problem 

Tags (1)
0 Kudos
Reply
4,006 Views
SorinIBancila
NXP Employee
NXP Employee

Hello,

I have a clean S32K1xx toolbox installed and I am not able to reproduce your problem. Did you bring any modification the example? What MATLAB version do you use?

From the previous post, I see that you use the S32K1xx v4.3.0? Am I right?

Best regards

Sorin Bancila

0 Kudos
Reply
3,995 Views
premch2301
Contributor III

while installing MLTBX file, i am facing problem on the last step(verify MBD toolbox license).  due to that it is not installing completely. 

MBT version: 

4.3.0 Model-Based Design Toolbox for S32K1xx Automotive Microprocessors Family

 

MATLAB version: R2024b

boot serial no: 92E107F3

license file : (.dat)

#Model-Based Design Toolbox for MATLAB/Simulink - Model-Based Design Toolbox
#for S32K1xx Automotive Microprocessors Family for Prem chanchal Software
#Account
# License for DISK_SERIAL_NUM=92E107F3 laptop
INCREMENT MC_Toolbox_S32K freescale 1.0 26-mar-2045 uncounted \
VENDOR_STRING="Model-Based Design Toolbox for S32K1xx \
Automotive Microprocessors Family" \
HOSTID=DISK_SERIAL_NUM=92e107f3 ISSUER="Freescale \
Semiconductor" ISSUED=02-apr-2025 ck=209 SN="FSL - 16070981" \
TS_OK SIGN="010D EDBB 08E4 D16D 281A 2570 AEB1 3280 2DBC 5852 \
2D0D 3BDF A9F0 32F4 75C3 1DB9 CF8C EE59 7D39 3F0F 61FE BD61 \
6119 AD4D C9B9 EEF8 9348 7117 20FE 82BF"

 

premch2301_0-1743682268427.png

 

0 Kudos
Reply
3,982 Views
SorinIBancila
NXP Employee
NXP Employee

Hello,

Unfortunately I am unable to reproduce your problem. No matter what I try, I can't get the same error.

In one of your screenshots, I saw that you have multiple S32K1xx toolboxes installed. Please make sure only on in installed.

Can you try these steps, maybe they solve the problem:

1. Revert the MATLAB Path to the Default one.

SorinIBancila_0-1743686026322.png

 

2. Uninstall all S32K1xx toolboxes. Navigate to the C:\Users\TPEM_USER_1\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes and delete all NXP_MBDToolbox_S32K1xx folder.

3. Restart MATLAB.

4. Go to Preferences -> MATLAB -> Add-Ons and modify the default installation folder to a shorter path and without including spaces . (e.g. C:\MATLAB\Addons\Toolboxes\R2024B)

5. Inside the MATLAB, navigate to the NXP_MBDToolbox_S32K1xx_4.3.0_20220913.mltbx file and double click on it and install the toolbox.

6. Manually activate the toolbox by copying the license.dat file inside the lic folder.

7. Run the mbd_s32k_path script.

 

Let me know if these steps solve your problem.

Best regards,

Sorin Bancila

0 Kudos
Reply
3,936 Views
premch2301
Contributor III

premch2301_0-1743750176547.png

 

premch2301_1-1743750177123.png

 

premch2301_2-1743750177220.png

 

premch2301_3-1743750176643.png

 

premch2301_4-1743750177006.png

 

premch2301_5-1743750176842.png

 

 

 

i have installed only one S32K1xx add on tool. followed all the above steps.  Still this issue is coming

0 Kudos
Reply
3,915 Views
premch2301
Contributor III

premch2301_0-1743755330773.png

there is something issue with the license file. 

0 Kudos
Reply
3,909 Views
SorinIBancila
NXP Employee
NXP Employee
Hello,

I've sent you a private message. Please check it out.

Best regards,
Sorin Bancila
0 Kudos
Reply