S32K144EVB Simulink LIN Blockset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144EVB Simulink LIN Blockset

1,744件の閲覧回数
comodo77
Contributor I

Hi everyone, I am looking for a LIN Simulink Blockset where can I define TX/RX Message IDs and get the data directly. Has someone a suitable example or blockset for that?

Regards 

0 件の賞賛
返信
1 返信

1,609件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello comodo77‌,

Unfortunately we do not have support for LIN in our S32K14x toolbox - the only option to use it from within Simulink is to add your custom code (via System blocks - e.g. System outputs) in the model. For that you can use the S32K SDK package that comes installed with our toolbox. You can find documentation for the SDK in {MBDT_ROOT}/S32_Platform_SDK/doc/Start_here.html

Kind regards,

Razvan.

0 件の賞賛
返信