S32K144EVB/Generated code download issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144EVB/Generated code download issue

7,261件の閲覧回数
mohamed_benderr
Contributor II

Hi NXP MBDT team,

I tried several times to generate the code of a basic example "gpio_s32k144.mdl" and download it to the board without success (the code is well generated but the download process did not accomplished: it hangs at the following step

*** Created executable: gpio_s32k144.mot

### Successful completion of build procedure for model: gpio_s32k144

For your information

I use Matlab release 2019a

NXP Model-Based Design Toolbox for S32K1xx – version 4.1.0

The board is well connected and detected 

In target connection i tried to refresh the OpenSDA Drive Name =>  without success 

I have selected OpenSDA Drive Name "F:EVB-s32k144 =>  without success 

I tried also to type in the the corresponding Custom OpenSDA Drive Name => without success 

I have copied the gpio_s32k144.mot directly to the board  => without success  

With all the previous steps i can not run any application

Could you please help me to resolve this issue

Thanks in advance for your support 

0 件の賞賛
返信
12 返答(返信)

6,997件の閲覧回数
mohamed_benderr
Contributor II

Hi NXP,

The issue is now resolved. I'm able to import the generated code to S32DS and build it.

However, we still have the projects that use Motor Ctrl library not working.

Thank you so match for your support.

0 件の賞賛
返信

6,997件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

Here is a fix for the importer - to work with AMMCLib as well. Could you please confirm that everything works as expected?

You need to replace the following file:

{TOOLBOX_ROOT}/mbdtbx_s32k/mscript/utils/mbd_s32k_ds.p

Kind regards,

Razvan.

0 件の賞賛
返信

6,997件の閲覧回数
mohamed_benderr
Contributor II

Hi,

I have done what you requested

pastedImage_1.png

The green led next to the OpenSDA is ON

The LASTSTAT.TXT is empty, I don't know how i can join it as an attached file to the discussion 

pastedImage_2.png

I still have the issue, i can't flash the board directly from matlab

Thanks in advance for your support

0 件の賞賛
返信

6,995件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected] ,

I have provided a patch here for the importing of projects generated by our toolbox into S32Design Studio (Note: version 2.2 - the latest one available on nxp.com).

For the patch you'll have to update the following files (preferably you should have a backup for them, before overwriting them):

{TOOLBOX_ROOT}/mbdtbx_s32k/mscript/utils/mbd_s32k_copy_required_files.p

{TOOLBOX_ROOT}/mbdtbx_s32k/mscript/utils/mbd_s32k_ds.p

{TOOLBOX_ROOT}/mbdtbx_s32k/mbd_s32k_make_rtw_hook.p

{TOOLBOX_ROOT}/mbdtbx_s32k/mbd_s32k.tmf

Note: projects that need the AMMCLib library is still under investigation - it seems to be an issue with the linking in S32DS. For that you can not import it as is, you can just select the elf file to flash/debug on the target. I will be out of office the next week, but once I return I will continue the investigation and patch that as well.

Kind regards,

Razvan.

0 件の賞賛
返信

6,994件の閲覧回数
mohamed_benderr
Contributor II

Hi,

You find bellow the requested informations:

pastedImage_1.png

0 件の賞賛
返信

6,994件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

It seems we have the same version on the OpenSDA.

I attached a generated .mot file from the gpio examples. Please drag and drop in the new mounted disk and after that please send us the LASTSTAT.TXT file content. 

Also, please pay attention to the green led next to the OpenSDA because it provides a status, it is explained here https://www.nxp.com/docs/en/user-guide/OPENSDAUG.pdf .

Hope this helps,

Marius

0 件の賞賛
返信

6,993件の閲覧回数
mohamed_benderr
Contributor II

Hi,

You find blow the photo of  S32K144EVB jumper setup 

pastedImage_1.png

pastedImage_2.png

     Below the content of LASTSTAT.TXT file 

pastedImage_3.png

0 件の賞賛
返信

6,995件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

The OpenSDA contains an SDA_INFO.HTM. Can you please send me the content displayed under "Your Hardware information" like here:

pastedImage_1.png

You can try at the PEmicro website to see if there are any updates for the OpenSDA.

Also, you can try flashing the gpio generated mot file with the S32DS to see if the generated code works as expected. You don;t need to import the project, just flash the generated .mot file.

Hope this helps,

Marius

0 件の賞賛
返信

6,995件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

As far as I understand from your post, the .mot has been successfully generated. 

In target connection i tried to refresh the OpenSDA Drive Name =>  without success 

The refresh button will look for all the mounted devices, it will not select the one you need.

I have selected OpenSDA Drive Name "F:EVB-s32k144 =>  without success 

This is how it looks for me.

pastedImage_5.png

I tried also to type in the the corresponding Custom OpenSDA Drive Name => without success 

For the custom SDA name you need to type only the letter fo the mounted Drive. In my case is D, your case F

pastedImage_8.png

I have copied the gpio_s32k144.mot directly to the board  => without success  

From this reason I assume there is a problem with the board, maybe the jumpers are not right set. Make sure the S32K is powered up. For reset jumper, the J104 must be connected 1-2. If you want to power the CPU from the USB then the J107 must be set 2-3. If you want to power up the controller from external sources the J107 must be set 1-2. 

Marius 

0 件の賞賛
返信

6,995件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected] ,

When you connect the S32K144EVB to your computer, can you go to the mounted drive (F in the case you described) and share the contents of the following file?

LASTSTAT.TXT

Kind regards,

Razvan.

0 件の賞賛
返信

6,995件の閲覧回数
mohamed_benderr
Contributor II

Hi,

You find blow thea photo of your S32K144EVB jumper setup

pastedImage_1.png

0 件の賞賛
返信

6,995件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

And [email protected] ,

Can you also share with us a photo of your S32K144EVB jumper setup? And maybe a photo with the revision you have, just so we can replicate the exact scenario you are using.

Kind regards,

Razvan.

0 件の賞賛
返信