S32K144 with Function to call low level driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 with Function to call low level driver

8,766 Views
Narudol-T
Contributor III

Dear Sir,

 

I am trying to trial some basic software of LED drive for calling header file of S32K144.

I have tried follow below thread to implement, then the compilation was success.

However, the LED does not show.

https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...
The Simulink have 2 blocks for this purpose:

 

1) LED_Initialization : Setting up GPIO direction 

-------------------------------------------------------------------------------------------------------------------

function LED_Initialization

% TODO: Update the bccPath with your project full path
bccPath = coder.const('C:\SVN_Checkout\MATLAB\devkit_S32K144_TICK\src\led');
coder.updateBuildInfo('addSourcePaths', bccPath);

if( coder.target( 'Rtw' ) )
%% Adding header information to the generated code
coder.cinclude('led_peripheries.h');
coder.cinclude('led_mbdt.h');

%% Adding source files to MakeFile
coder.updateBuildInfo( 'addSourceFiles', 'led_peripheries.c' );
coder.updateBuildInfo( 'addSourceFiles', 'led_mbdt.c' );

%% Initializing the BCC driver
coder.ceval('MBD_LED_Initialization');

end

-------------------------------------------------------------------------------------------------------------------

2) LED_On : Write GPIO to be "LOW" for pull-down "RED LED" at PTD15

-------------------------------------------------------------------------------------------------------------------

function LED_On

if( coder.target( 'Rtw' ) )

coder.ceval('MBD_LED_On');

end
end

-------------------------------------------------------------------------------------------------------------------

Can you help advising which parts of code written wrong ?

 

Thanks in advanced

Narudol T.

0 Kudos
Reply
2 Replies

8,764 Views
Narudol-T
Contributor III

Add more pictures.

0 Kudos
Reply

6,882 Views
SuperBeginner
Contributor III

Hi @Narudol-T ,

I have the same needs as you.

I need to implement the LED function through a custom function.

Have the issues you encountered been resolved?

If so, how did you solve it? 

Could you help me, please?

 

Thanks in advance

0 Kudos
Reply