S32K144 license of motor control development toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 license of motor control development toolbox

2,968 Views
koyo_y
Contributor I

I am considering using the Motor control deveiopment toolbox for S32K144.
I am sorry that it became an elementary question.

There seems to be two kinds of trail licenses and permanent licenses(to purchase) in , but I did not know what kind of difference there is when actually using it.
Please tell me the difference between trail license and permanent license.

For example, Trial license has trial period up to 3 months\\\\

0 Kudos
Reply
3 Replies

2,768 Views
raduivan
NXP Employee
NXP Employee

Hi Shunsuke,

   The Toolbox is now free of charge, you can request a license using the following steps:

1. Go to www.nxp.com/mctoolbox

2. Click on ‘Get Product & License’
3. Login. If not registered yet, click register.

4.Product Information page appears. Click on 'Motor Control Toolbox for MATLAB/Simulink MBD supporting S32K'.

5. Click “I Agree” to consent to the software license agreement.

6. If you need to download the tool, click on the linked file name. Otherwise, click on “License Keys” tab.

Regards,

Radu

0 Kudos
Reply

2,766 Views
koyo_y
Contributor I

Dear Radu

Thank you for your reply.

I am sorry that the explanation is insufficient.

This question is an inquiry from our customers.

We do not need licenses for distributors.

Customers are considering using Motor control development toolbox and have not obtained a license yet.

Customers are investigating how much it costs before using this toolbox.

Therefore, it is said that you want us to tell you the difference between trial and purchase licenses in the attached document.

For example, if you are a free Trial license you can only use for a short period of time, no technical support , etc.

Best regards

Shunsuke Yamaura

0 Kudos
Reply

2,766 Views
raduivan
NXP Employee
NXP Employee

Hi Shunsuke,

   The Toolbox it self now is free, the customer can use it free of charge not time limited and no technical support included. In the past we had those two versions trial and purchased but that scheme now is absolute. So the customers will not have to pay anything for the MBD Toolbox license.

   Let me know if you need more information.

Best regards,

Radu

0 Kudos
Reply