S32K144: Is there a way to use FlexIO pin for PWM generation in Simulink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144: Is there a way to use FlexIO pin for PWM generation in Simulink

ソリューションへジャンプ
468件の閲覧回数
mirali
Contributor I

Currently trying to figure out how to use a FlexIO pin for PWM generation in Simulink. I don't see any blocks in Simulink for using a FlexIO pin for PWM generation, only for I2C, SPI and UART. Any help would be greatly appreciated. 

0 件の賞賛
返信
1 解決策
428件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @mirali ,

Unfortunately, in MBDT for S32K1xx, for the FlexIO we do not provide PWM generation blocks. However, such support can be achieved by using custom code in a similar approach described by this article: https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...

I am not sure if the S32K1 SDK, the abstraction layer on which the MBDT for S32K1 generates the hardware access peripherals code has such support for the PWM generation, so in this case you can directly control and achieve such functionality by writing to registers using a similar approach mentioned in the article above.

Regards,

Marius

元の投稿で解決策を見る

2 返答(返信)
429件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @mirali ,

Unfortunately, in MBDT for S32K1xx, for the FlexIO we do not provide PWM generation blocks. However, such support can be achieved by using custom code in a similar approach described by this article: https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...

I am not sure if the S32K1 SDK, the abstraction layer on which the MBDT for S32K1 generates the hardware access peripherals code has such support for the PWM generation, so in this case you can directly control and achieve such functionality by writing to registers using a similar approach mentioned in the article above.

Regards,

Marius

418件の閲覧回数
mirali
Contributor I

Thank you for the information

0 件の賞賛
返信