S32K MBD Toolbox software Build Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K MBD Toolbox software Build Error

Jump to solution
4,523 Views
李风heart
Contributor II

Hi:

I have just installed MBDToolbox_S32K1xx_v3.0.0_20171016 on my computer. And I got a lincense.bat from this page.

pastedImage_1.png.

 But while I build gpio_s32k14.mdl there is something wrong .pastedImage_3.png.

I also Installed TDM-GCC V5.1 and creat environment variables like this.

pastedImage_2.png

How to solve this error, did anyone have suggestions ?

Thanks

Li Feng

Labels (1)
Tags (1)
1 Solution
4,169 Views
wjandsq
Contributor IV

the toolchain  is error,  TDM-GCC V5.1 is for windows x86/x64 C Compile, Windows API libraries, not for S32K。

View solution in original post

5 Replies
4,170 Views
wjandsq
Contributor IV

the toolchain  is error,  TDM-GCC V5.1 is for windows x86/x64 C Compile, Windows API libraries, not for S32K。

4,169 Views
thomsonzhou
Contributor III

You need a head file for compile this project successfully. You can ask them for this file for your projects.

Thomson

0 Kudos
Reply
4,169 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Li Feng, 

Do you have any particular reasons for installing the version 3.0.0 and not the latest one https://community.nxp.com/docs/DOC-341052  ? 

Best regards,

Daniel

0 Kudos
Reply
4,169 Views
李风heart
Contributor II

Hi Daniel,

Thanks for your attention.

Because our office is using this version of MBD and using the same version of MBD makes the project better versatile on different computers.

Thanks

Li Feng

0 Kudos
Reply