Running M4 demo application on i.MX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running M4 demo application on i.MX8

1,412件の閲覧回数
kumar_praveen
Contributor II

Hi,

I am using Linux 4.14.98.2.0.0, SCFW 1.2 and MCU expresso SDK_2.5.2.

I am trying to run the freeRTOS demo application demo_apps/hello_world. At the time of flashing emmc (In serial mode) I could see the "hello world" print; but when I change the mode to EMMC boot mode, I am could only the below messages:

####################  CODEC SRTM DEMO ####################    

Build Time: Mar 25 2019--15:31:14

##########################################################

Press 'r' to do M4 partition reset

r

Wait a while to reboot

####################  CODEC SRTM DEMO ####################

I do not see the hello world message again; even after reboot the "hello world" message doesn't print.

Please clarify.

Regards,

Praveen

0 件の賞賛
返信
1 返信

1,124件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello kumar.praveen@sasken.com‌,

On this community we handle questions regarding MATLAB/Simulink and our toolboxes. I would suggest you move your question on the I.MX community.

Kind regards,

Razvan.

0 件の賞賛
返信