Restart PIL Simulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Restart PIL Simulation

2,383 Views
hnkChinaski
Contributor I

Hi,

I'm doing PIL simulations and everything works fine. However, downloading the application to the board using the RAppID bootloader everytime I rerun a simulation takes a long time.

Is there a way to simply restart the simulation in Simulink without needing to download the same model again to the board?

Thank you

0 Kudos
Reply
2 Replies

2,296 Views
hnkChinaski
Contributor I

Hi,

I don't think the fast restart option helps with my problem. If I rerun a simulation with fast restart activated, the RAppID Bootlader will reflash the application first.

0 Kudos
Reply

2,355 Views
patrick_schmid
Contributor I

Hi,

I'm facing the same issue. Or is there an option to bypass the flashing with the RAppID bootlader, e.g., by use S32 Design Studio to flash the board and "just" run the PiL simulation in Simulink?
Thanks for your answers.

0 Kudos
Reply