Restart PIL Simulation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Restart PIL Simulation

2,405件の閲覧回数
hnkChinaski
Contributor I

Hi,

I'm doing PIL simulations and everything works fine. However, downloading the application to the board using the RAppID bootloader everytime I rerun a simulation takes a long time.

Is there a way to simply restart the simulation in Simulink without needing to download the same model again to the board?

Thank you

0 件の賞賛
返信
2 返答(返信)

2,318件の閲覧回数
hnkChinaski
Contributor I

Hi,

I don't think the fast restart option helps with my problem. If I rerun a simulation with fast restart activated, the RAppID Bootlader will reflash the application first.

0 件の賞賛
返信

2,377件の閲覧回数
patrick_schmid
Contributor I

Hi,

I'm facing the same issue. Or is there an option to bypass the flashing with the RAppID bootlader, e.g., by use S32 Design Studio to flash the board and "just" run the PiL simulation in Simulink?
Thanks for your answers.

0 件の賞賛
返信