Request for Support on SPI Communication Issue – Follow-up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for Support on SPI Communication Issue – Follow-up

1,342件の閲覧回数
Vijay98
Contributor II

Hello, NXP Team

I apologize for the follow-up.

A week has passed since I brought up the SPI communication issue in the following thread, along with an example model:

SPI communication issue with example model - NXP Community

Since we need to finish setting up SPI communication, we would be very grateful for your help in fixing this problem.

I appreciate your help in advance.

 

Thanks & Regards,

Vijay

0 件の賞賛
返信
1 返信

1,315件の閲覧回数
stefanvlad
NXP Employee
NXP Employee

Hi @Vijay98 ,

 

I have replied to your post SPI communication issue with example model - NXP Community

Please use that thread and avoid starting new threads for the same topic,

 

Regards,
Stefan V.

0 件の賞賛
返信