Request for Support on SPI Communication Issue – Follow-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for Support on SPI Communication Issue – Follow-up

1,340 Views
Vijay98
Contributor II

Hello, NXP Team

I apologize for the follow-up.

A week has passed since I brought up the SPI communication issue in the following thread, along with an example model:

SPI communication issue with example model - NXP Community

Since we need to finish setting up SPI communication, we would be very grateful for your help in fixing this problem.

I appreciate your help in advance.

 

Thanks & Regards,

Vijay

0 Kudos
Reply
1 Reply

1,313 Views
stefanvlad
NXP Employee
NXP Employee

Hi @Vijay98 ,

 

I have replied to your post SPI communication issue with example model - NXP Community

Please use that thread and avoid starting new threads for the same topic,

 

Regards,
Stefan V.

0 Kudos
Reply