Regarding 32 bytes of data transmission from MBDT toolbox [can-fd] -Simulink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding 32 bytes of data transmission from MBDT toolbox [can-fd] -Simulink

625 Views
KavithaSasikumar
Contributor I

HI,

I am working with S32k144 and s32k344 boards. I have already implemented normal can 8 bytes communication for automotive use cases via s32k144 board. But now when i try to work for 32 bytes of data transfer over nxp mbdt toolbox along with Vehicle network toolbox support, i couldn't get the data out in my TS masters/canoe platform. Virtually inside MATLAB i am able to receive it. Kindly make sure if its nxp mbdt over Simulink supports 32 bytes of data transmission via can fd or not? if so do provide me some links to refer please.

0 Kudos
Reply
1 Reply

541 Views
Adrian_Gherca
NXP Employee
NXP Employee

Hello and thank you for yout interest in MBDT.

In case of S32k144, please confirm that you have tried setting the payload size to 32 bytes in the FCAN_Config block, like this:

Adrian_Gherca_0-1729497355931.png



For s32k3xx the CAN communication can no longer be configured from the Config block but using a configuration project: EB Tresos or S32 Configuration Tool.

0 Kudos
Reply