Read a dbc file directly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Read a dbc file directly

ソリューションへジャンプ
3,871件の閲覧回数
fra_rio
Contributor I

Hello,

is there the possibility to read a dbc-file directly with a block from NXP's Model-Based-Design-Toolbox (Without any additional toolboxes from MathWorks)?

I use the NXP S32K144 EVB.

Thanks,

Frank

タグ(1)
0 件の賞賛
返信
1 解決策
3,694件の閲覧回数
fra_rio
Contributor I

Do I understand it right, that it is not possible to read a dbc-file directly without any other toolboxes or converters?

元の投稿で解決策を見る

3 返答(返信)
3,694件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi fra_rio‌

NXP's Model-Based Design Toolbox allows you to read any raw data that is transmitted via CAN/CAN-FD to a particular node. If you wish to convert the data to a human readable format you can use any standard Simulink library block (no additional toolbox required) or if you have the C-source code that performs such conversion you can call it directly in Simulink alongside the NXP MBDT.

Here is a good resource that explains the conversion mechanism if you wish to implement it.

Hope it helps!

Daniel

0 件の賞賛
返信
3,695件の閲覧回数
fra_rio
Contributor I

Do I understand it right, that it is not possible to read a dbc-file directly without any other toolboxes or converters?

3,694件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Correct!

0 件の賞賛
返信