Re: i.MX RT - How To

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: i.MX RT - How To

2,866件の閲覧回数
Leon_Li1
NXP Employee
NXP Employee

Hi,

I have installed MBDT successfully, I can generated code use the default folder path.

But if I move the gpio_polling example to a new folder, I cant build it ok.

The message as below:

Build Summary 

1
Elapsed: 0.4 sec
Top model targets built: Model Action Rebuild Reason ====================================================================================== evkmimxrt1060_gpio_polling Failed Code generation information file does not exist. 0 of 1 models built (0 models already up to date) Build duration: 0h 0m 3.639s
文件标识符无效。使用 fopen 生成有效的文件标识符。
 
Matlab version is 2021a.
MBDT version is 1.2.0
0 件の賞賛
返信
4 返答(返信)

2,835件の閲覧回数
Leon_Li1
NXP Employee
NXP Employee

Hi Alexandra,

I have a new qustion.

When I built the mc_pmsm example, the report massage as below:

MotorC_0-1629978529718.png

If I use Matlab 2020a, this example can be built successfully,but matlab 2021a cant.

0 件の賞賛
返信

2,798件の閲覧回数
nxa11767
NXP Employee
NXP Employee

Hi @Leon_Li1 ,

We have a fix for the build error on 2021a. 

Please find the attached zip file - it contains a .tcl file. Unzip it and copy the file to: RTCESL_imxrt\bam\AMCLIB\bam_a32fltfltflt\ and overwrite the existing one: AMCLIB_PMSMBemfObsrvDQ_SF_A32fff.tlc.

 

Best regards,

Alexandra

0 件の賞賛
返信

2,839件の閲覧回数
Leon_Li1
NXP Employee
NXP Employee

It is ok, thanks for your help.

0 件の賞賛
返信

2,853件の閲覧回数
nxa11767
NXP Employee
NXP Employee

Hi @Leon_Li1 ,

Did you extended error look like below?

nxa11767_0-1629966558968.png

This is caused by the initial model being created with an older version of matlab, and some things changed in the data storage options.

To fix the issue click on a small icon in the left lower corner, to open the model perspectives:

nxa11767_1-1629967151654.png

Enter the Code perspective, and in Data storage type, fix the error for the 'A' storage variable:

nxa11767_2-1629967399086.png

 

Hope this helps,

Alexandra

0 件の賞賛
返信