RDVCU5775EVM MBDT cannot flash via RAppID in Simulink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RDVCU5775EVM MBDT cannot flash via RAppID in Simulink

746 次查看
cswh
Contributor I

RDVCU5775EVM MPC5775B-E 

Env:

- Board: RDVCU5775EVM

- Software:  S32DS.Power.2.1 + Matlab2022B + PPROGPPCNEXUS

- MBDT Package:

        MBDToolbox_MPC57xx_3.2.0_20200414.mltbx

        NXP_Support_Package_MPC57xx_20200414.mltbx

 

Problem Description:

1. Before 2024.8.1, I had flashed bootloader, successfully deployed MBDT generated ELFs many times via S32DS and via RAppID (in Simulink) . (Following Solved: Unable to Flash MBDT BootLoader to RDVCU5775EVM in S32DS per Quick Start Guide - NXP Communi...)

2. At 2024.8.1, I cannot do any flash, it stuck at 99% like this:

cswh_0-1722928926951.png

I found it is similar to this problem Solved: Unable to start debug session on MPC5748G board. download stops at 98% - NXP Community

so I used PPROGPPCNEXUS to earse flash.

3. After that, I can flash bootloader and Elf via S32DS, and the deployed programs run normally in board.

But it fails every time when I try to deploy MBDT generated ELFs via RAppID (in Simulink) , like this:

cswh_1-1722929325618.png

PS: I set device Name="MPC5777C" in S32DS  and set Target="MPC5775B" in MBDT, it works fine. After this problem occurred, I tried all "MPC5777C" and all "MPC5775B", nothing happened.

Is there something I have done wrong ? Or what can I do to make everything right ?

 

 

 

0 项奖励
回复
0 回复数