RAM/FLASH ECC error FCCU Fault injection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAM/FLASH ECC error FCCU Fault injection

2,751 Views
akhil_kumar
Contributor I

How to inject RAM ECC NCF fault for FCCU?

is there any example available to create a RAM/FLASH ECC fault ?

Regards

Akhil

Labels (2)
0 Kudos
Reply
3 Replies

2,573 Views
akhil_kumar
Contributor I

Hi Razvan,

We can provide basic configuration understanding of FCCU driver.

 

Thanks

Akhil 

0 Kudos
Reply

2,571 Views
akhil_kumar
Contributor I

Hi Chivu,

Thanks for your reply

We are testing RAM ECC with our custom code,However still not able to insert fault at MEMU and FCCU level simultaneously.Hereby i am attaching sample code and dumped configuration for your reference.Please look into it for your reference and help us in this regards.

 

Thanks

Akhil 

0 Kudos
Reply

2,571 Views
constantinrazva
NXP Employee
NXP Employee

Hello,

Unfortunately we do not have such an example as we do not have support for FCCU. The only way this would be possible is by inserting custom code into your model. If you want to go with this approach and are facing issues, please let us know. We can help on the MATLAB/Simulink side, but we do not have expertise on the FCCU driver side.

Kind regards,

Razvan.

0 Kudos
Reply