Qusetion about DEVKIT-MPC5744P MBD toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Qusetion about DEVKIT-MPC5744P MBD toolbox

2,000件の閲覧回数
260068845
Contributor III

Hello,
I used the DEVKIT-MPC5744P MBD toolbox for application development and found the following two problems.
1. When doing the PIL test, after compiling the model and downloading it to the development board using OPENSDA, the following error occurred. What may be the reason?QQ截图20190516112534.png
2. The CAN0 on the development board is connected to the external CAN network, and communication is impossible. When CAN1 is connected to the external TJA1050 chip, communication can be performed. What may be the problem?

0 件の賞賛
返信
1 返信

1,891件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

For the first question, could you share the model you are using to see what the problem is with running PIL mode? You can share a stripped version of the model if you cannot share all of it, just so I can replicate the issue. That error means that the protocol Simulink uses for PIL communication is not respected by both parties [host PC and embedded target].

For the second question, could you give me some more details so I can test it on your setup? Or as close I can get to it on my side.

Kind regards,

Razvan.

0 件の賞賛
返信