Quadrature encoder block in simulink support package for FRDM-K64F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Quadrature encoder block in simulink support package for FRDM-K64F

4,386 Views
s276141
Contributor I

Goodmorning, 

I've some doubts about the block in the photo. I'm trying to control an electric motor via model-based software design. I want to obtain the ticks count and the direction thanks to a quadrature encoder. However, I don't know which GPIO pins to use, since this block doesn't let me choose them. Are there pre defined pins to use with a quadrature encoder on this board? Do you have some hint? 

Labels (2)
0 Kudos
Reply
1 Reply

4,298 Views
constantinrazva
NXP Employee
NXP Employee

Hello s276141@studenti.polito.it ,

Unfortunately we do not handle questions regarding that toolbox - I suggest you post your question here Simulink Coder Support Package for NXP FRDM-K64F Board - File Exchange - MATLAB Central  where you'll find someone that can help.

Kind regards,

Razvan.

0 Kudos
Reply