Pwm_lcu_pins_config_issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pwm_lcu_pins_config_issue

631 次查看
MN_TL_24
Contributor I

Hello Nxp team,

We are also working in Pwm_trigmux_lcu to generate the pwm pulse in Lcu pins.

And we have checked the model given by nxp team in this post - Re: Pwm_delay_in_trigger_pulse - NXP Community ; "s32k312_pwm_lcu_mod_carrier_s32ct.zip" and we have also used 'PTA0' as the High side pin 

but we need to configure the 'PTC10' pin as the Low side pin, but we can't be able to see the waveform in Ptc 10 pin.

we have attached the photos by steps of which we configured.

 

Step-1: Pin configuration 

MN_TL_24_0-1732163479401.png

 

 

Step-2: Pin config in port driver

MN_TL_24_1-1732163479701.png

 

 

Step-3: Pwm driver configuration

MN_TL_24_2-1732163479368.png

 

MN_TL_24_3-1732163479592.png

 

 

Step-4: Trigmux configuration for Ptc10 (Lcu1_out11)

MN_TL_24_4-1732163479428.png

 

 

Step-5: Lcu_instance configuration

MN_TL_24_5-1732163479679.png

 

 

Step-6: Lcu logic input config

MN_TL_24_6-1732163479585.png

 

 

Step-7: Lcu logic output configuration

MN_TL_24_7-1732163479549.png

 

Kindly check this configuration, we think that we have made some small mistake in this.

We want to generate High side pwm pulse in "PTA0" - this is ok

and Low side PWM pulse in "PTC10" - this we tried but the waveform is not able to view.

 

Kindly help us to resolve this issue.

 

Thanks & regards,

MN_TL

0 项奖励
回复
2 回复数

562 次查看
stefanvlad
NXP Employee
NXP Employee

Hi @MN_TL_24 , @Vijay98 

 

Thank you for reading the post,

I have responded in the same thread Re: Pwm_delay_in_trigger_pulse - NXP Community

And i recommend we keep the discussions in the same thread, as above, and do not open multiple threads with same topic,

 

Hope this solves your questions,

Best regards,

Stefan V.

0 项奖励
回复

586 次查看
MN_TL_24
Contributor I

Hello NXP team, 

Any update for configuring the PTC 10 pin for the above lcu pin configuration.

 

Kindly help us to resolve this issue.

@stefanvlad @Vijay98 

0 项奖励
回复