Program upload to RDVCU5775EVM board via CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program upload to RDVCU5775EVM board via CAN

1,256 Views
peaces
Contributor III

We want to install a program with Can Bus, but there is no information on how to access the OpenBus application mentioned in the user manual, can you give us some information on how to proceed?

0 Kudos
Reply
1 Reply

1,252 Views
Dong_Luo
NXP Employee
NXP Employee

hello @peaces 

The OpenBus tool follows the UDS protocol, a communication protocol used for ECU diagnosis, and it only supports the PCAN-USB devices for downloading programs to RDVCU5775EVM.

nxf47394_0-1624088631896.png

 

We provide the SDK-based bootloader and application demo instead of MBDT. In addition, the package size of the OpenBus is about 78MB. Please submit a new ticket if you want it.