Problem reported by customer when installing S32K1xx version 4.2.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem reported by customer when installing S32K1xx version 4.2.3

Jump to solution
1,635 Views
nxp52415
NXP Employee
NXP Employee

Hello,

This is Hector here, customer is seeing a problem when upgrading to version 4.2.3 and I would like to know whether somebody has expereinced something similar. Below description, thanks.

 

I have problem after installing  (MBDT for S32K1xx Series Version : 4.2.3 (R2016a-R2020a)), before I was using Version 4.2.2. But after upgrading to 4.2.3, The following problem appears to me while generating a code.

nxp52415_0-1669902278474.pngnxp52415_0-1669902278474.png

 

 

I compared with Björn, but he don’t have this issue. I suppose, that something went wrong after upgrading to Version: 4.2.3

 

Could you please support?

 

Just for info, this is the MBDToolbox patch that I used to install the package.

nxp52415_1-1669902278502.pngnxp52415_1-1669902278502.png

 

0 Kudos
Reply
1 Solution
1,618 Views
nxp52415
NXP Employee
NXP Employee

The problem described by the customer can be solved by updating to the toolbox to version 4.3.0.

The issue was resolved in internal task number AST-3351.

 

View solution in original post

0 Kudos
Reply
1 Reply
1,619 Views
nxp52415
NXP Employee
NXP Employee

The problem described by the customer can be solved by updating to the toolbox to version 4.3.0.

The issue was resolved in internal task number AST-3351.

 

0 Kudos
Reply