Problem reported by customer when installing S32K1xx version 4.2.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem reported by customer when installing S32K1xx version 4.2.3

ソリューションへジャンプ
1,627件の閲覧回数
nxp52415
NXP Employee
NXP Employee

Hello,

This is Hector here, customer is seeing a problem when upgrading to version 4.2.3 and I would like to know whether somebody has expereinced something similar. Below description, thanks.

 

I have problem after installing  (MBDT for S32K1xx Series Version : 4.2.3 (R2016a-R2020a)), before I was using Version 4.2.2. But after upgrading to 4.2.3, The following problem appears to me while generating a code.

nxp52415_0-1669902278474.pngnxp52415_0-1669902278474.png

 

 

I compared with Björn, but he don’t have this issue. I suppose, that something went wrong after upgrading to Version: 4.2.3

 

Could you please support?

 

Just for info, this is the MBDToolbox patch that I used to install the package.

nxp52415_1-1669902278502.pngnxp52415_1-1669902278502.png

 

0 件の賞賛
返信
1 解決策
1,610件の閲覧回数
nxp52415
NXP Employee
NXP Employee

The problem described by the customer can be solved by updating to the toolbox to version 4.3.0.

The issue was resolved in internal task number AST-3351.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,611件の閲覧回数
nxp52415
NXP Employee
NXP Employee

The problem described by the customer can be solved by updating to the toolbox to version 4.3.0.

The issue was resolved in internal task number AST-3351.

 

0 件の賞賛
返信