PIL TEST

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PIL TEST

3,147 次查看
kunpeng_guo
Contributor I

Hi, MBDTeam, I have a S32K118 Board, When I Open the example in "NXP_MBDToolbox_S32K1xx"  folder, I want to make the PIL test, but I get the follows messages on the "Diagnostic View"

### Generating code into build folder: C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\slprj\mbd_s32k14\sim_pil_target_AMMCLIB_s32k14x ### Invoking Target Language Compiler on sim_pil_target_AMMCLIB_s32k14x.rtw ### Using System Target File: C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\mbdtbx_s32k14x\mbdtbx_s32k14x\mbd_s32k14.tlc ### Using Model-Based Design Toolbox for S32K1xx Series 2018.R1 (R2016b-R2018a) 23-Jul-2018
### Loading TLC function libraries ...... ### Initial pass through model to cache user defined code ### Caching model source code .......................... ### Writing header file sim_pil_target_AMMCLIB_s32k14x_types.h ### Writing header file sim_pil_target_AMMCLIB_s32k14x.h . ### Writing source file sim_pil_target_AMMCLIB_s32k14x.c ### Writing header file sim_pil_target_AMMCLIB_s32k14x_private.h ### Writing header file rtiostream_uart_init.h ### Writing source file rtiostream_uart_init.c ### Writing source file mbd_hw_init.c ### TLC code generation complete. CGIR assertion 'begin != 0' failed in 'b:\matlab\toolbox\coder\trace\src\trace\traceutil.cpp:302' [ 0] 0x000000011f9feabf bin\win64\libmwtrace.dll+00191167 mwboost::archive::codecvt_null<wchar_t>::codecvt_null<wchar_t>+00002783 [ 1] 0x000000011faa761b bin\win64\libmwtrace.dll+00882203 coder::trace::TraceInfoBuilder::setTraceDelim+00088731 [ 2] 0x000000011fa9d8c0 bin\win64\libmwtrace.dll+00841920 coder::trace::TraceInfoBuilder::setTraceDelim+00048448 [ 3] 0x000000011fa7fbf7 bin\win64\libmwtrace.dll+00719863 coder::trace::TraceInfoBuilder::extractTraceInfo+00000263 [ 4] 0x000000011fac6706 bin\win64\libmwtrace.dll+01009414 coder::trace::TraceInfoBuilder::setTraceDelim+00215942 [ 5] 0x000000001cb93c60 bin\win64\pgo\mcos_impl.dll+00408672 [ 6] 0x000000001cb93232 bin\win64\pgo\mcos_impl.dll+00406066 [ 7] 0x000000001cb9234b bin\win64\pgo\mcos_impl.dll+00402251 [ 8] 0x000000001cb90d12 bin\win64\pgo\mcos_impl.dll+00396562 [ 9] 0x000000001cbe6f30 bin\win64\pgo\mcos_impl.dll+00749360 [ 10] 0x000000001cde3585 bin\win64\pgo\mcos_impl.dll+02831749 mwboost::serialization::singleton_module::unlock+01534417 [ 11] 0x000000001cdecf01 bin\win64\pgo\mcos_impl.dll+02871041 mwboost::serialization::singleton_module::unlock+01573709 [ 12] 0x0000000006cc3655 bin\win64\mcos.dll+00144981 omDirectCallMethod+00000069 [ 13] 0x0000000015af75c2 bin\win64\pgo\libmwlxeindexing.dll+00357826 MathWorks::lxe::MatrixModuleImplementation::SetHeterogeneousArray+00014702 [ 14] 0x0000000015b78936 bin\win64\pgo\libmwlxeindexing.dll+00887094 MathWorks::lxe::assign_paren_shared_xvalue_ptr_uninitialized_to_struct+00006890 [ 15] 0x0000000015aac70f bin\win64\pgo\libmwlxeindexing.dll+00050959 MathWorks::lxe::at_rbrace_nargout+00006831 CGIR assertion 'begin != 0' failed in 'b:\matlab\toolbox\coder\trace\src\trace\traceutil.cpp:302' [ 0] 0x000000011f9feabf bin\win64\libmwtrace.dll+00191167 mwboost::archive::codecvt_null<wchar_t>::codecvt_null<wchar_t>+00002783 [ 1] 0x000000011faa761b bin\win64\libmwtrace.dll+00882203 coder::trace::TraceInfoBuilder::setTraceDelim+00088731 [ 2] 0x000000011fa9d8c0 bin\win64\libmwtrace.dll+00841920 coder::trace::TraceInfoBuilder::setTraceDelim+00048448 [ 3] 0x000000011fa7fbf7 bin\win64\libmwtrace.dll+00719863 coder::trace::TraceInfoBuilder::extractTraceInfo+00000263 [ 4] 0x000000011fac6706 bin\win64\libmwtrace.dll+01009414 coder::trace::TraceInfoBuilder::setTraceDelim+00215942 [ 5] 0x000000001cb93c60 bin\win64\pgo\mcos_impl.dll+00408672 [ 6] 0x000000001cb93232 bin\win64\pgo\mcos_impl.dll+00406066 [ 7] 0x000000001cb9234b bin\win64\pgo\mcos_impl.dll+00402251 [ 8] 0x000000001cb90d12 bin\win64\pgo\mcos_impl.dll+00396562 [ 9] 0x000000001cbe6f30 bin\win64\pgo\mcos_impl.dll+00749360 [ 10] 0x000000001cde3585 bin\win64\pgo\mcos_impl.dll+02831749 mwboost::serialization::singleton_module::unlock+01534417 [ 11] 0x000000001cdecf01 bin\win64\pgo\mcos_impl.dll+02871041 mwboost::serialization::singleton_module::unlock+01573709 [ 12] 0x0000000006cc3655 bin\win64\mcos.dll+00144981 omDirectCallMethod+00000069 [ 13] 0x0000000015af75c2 bin\win64\pgo\libmwlxeindexing.dll+00357826 MathWorks::lxe::MatrixModuleImplementation::SetHeterogeneousArray+00014702 [ 14] 0x0000000015b78936 bin\win64\pgo\libmwlxeindexing.dll+00887094 MathWorks::lxe::assign_paren_shared_xvalue_ptr_uninitialized_to_struct+00006890 [ 15] 0x0000000015aac70f bin\win64\pgo\libmwlxeindexing.dll+00050959 MathWorks::lxe::at_rbrace_nargout+00006831 CGIR assertion 'begin != 0' failed in 'b:\matlab\toolbox\coder\trace\src\trace\traceutil.cpp:302' [ 0] 0x000000011f9feabf bin\win64\libmwtrace.dll+00191167 mwboost::archive::codecvt_null<wchar_t>::codecvt_null<wchar_t>+00002783 [ 1] 0x000000011faa761b bin\win64\libmwtrace.dll+00882203 coder::trace::TraceInfoBuilder::setTraceDelim+00088731 [ 2] 0x000000011fa9d8c0 bin\win64\libmwtrace.dll+00841920 coder::trace::TraceInfoBuilder::setTraceDelim+00048448 [ 3] 0x000000011fa7fbf7 bin\win64\libmwtrace.dll+00719863 coder::trace::TraceInfoBuilder::extractTraceInfo+00000263 [ 4] 0x000000011fac6706 bin\win64\libmwtrace.dll+01009414 coder::trace::TraceInfoBuilder::setTraceDelim+00215942 [ 5] 0x000000001cb93c60 bin\win64\pgo\mcos_impl.dll+00408672 [ 6] 0x000000001cb93232 bin\win64\pgo\mcos_impl.dll+00406066 [ 7] 0x000000001cb9234b bin\win64\pgo\mcos_impl.dll+00402251 [ 8] 0x000000001cb90d12 bin\win64\pgo\mcos_impl.dll+00396562 [ 9] 0x000000001cbe6f30 bin\win64\pgo\mcos_impl.dll+00749360 [ 10] 0x000000001cde3585 bin\win64\pgo\mcos_impl.dll+02831749 mwboost::serialization::singleton_module::unlock+01534417 [ 11] 0x000000001cdecf01 bin\win64\pgo\mcos_impl.dll+02871041 mwboost::serialization::singleton_module::unlock+01573709 [ 12] 0x0000000006cc3655 bin\win64\mcos.dll+00144981 omDirectCallMethod+00000069 [ 13] 0x0000000015af75c2 bin\win64\pgo\libmwlxeindexing.dll+00357826 MathWorks::lxe::MatrixModuleImplementation::SetHeterogeneousArray+00014702 [ 14] 0x0000000015b78936 bin\win64\pgo\libmwlxeindexing.dll+00887094 MathWorks::lxe::assign_paren_shared_xvalue_ptr_uninitialized_to_struct+00006890 [ 15] 0x0000000015aac70f bin\win64\pgo\libmwlxeindexing.dll+00050959 MathWorks::lxe::at_rbrace_nargout+00006831 CGIR assertion 'begin != 0' failed in 'b:\matlab\toolbox\coder\trace\src\trace\traceutil.cpp:302' [ 0] 0x000000011f9feabf bin\win64\libmwtrace.dll+00191167 mwboost::archive::codecvt_null<wchar_t>::codecvt_null<wchar_t>+00002783 [ 1] 0x000000011faa761b bin\win64\libmwtrace.dll+00882203 coder::trace::TraceInfoBuilder::setTraceDelim+00088731 [ 2] 0x000000011fa9d8c0 bin\win64\libmwtrace.dll+00841920 coder::trace::TraceInfoBuilder::setTraceDelim+00048448 [ 3] 0x000000011fa7fbf7 bin\win64\libmwtrace.dll+00719863 coder::trace::TraceInfoBuilder::extractTraceInfo+00000263 [ 4] 0x000000011fac6706 bin\win64\libmwtrace.dll+01009414 coder::trace::TraceInfoBuilder::setTraceDelim+00215942 [ 5] 0x000000001cb93c60 bin\win64\pgo\mcos_impl.dll+00408672 [ 6] 0x000000001cb93232 bin\win64\pgo\mcos_impl.dll+00406066 [ 7] 0x000000001cb9234b bin\win64\pgo\mcos_impl.dll+00402251 [ 8] 0x000000001cb90d12 bin\win64\pgo\mcos_impl.dll+00396562 [ 9] 0x000000001cbe6f30 bin\win64\pgo\mcos_impl.dll+00749360 [ 10] 0x000000001cde3585 bin\win64\pgo\mcos_impl.dll+02831749 mwboost::serialization::singleton_module::unlock+01534417 [ 11] 0x000000001cdecf01 bin\win64\pgo\mcos_impl.dll+02871041 mwboost::serialization::singleton_module::unlock+01573709 [ 12] 0x0000000006cc3655 bin\win64\mcos.dll+00144981 omDirectCallMethod+00000069 [ 13] 0x0000000015af75c2 bin\win64\pgo\libmwlxeindexing.dll+00357826 MathWorks::lxe::MatrixModuleImplementation::SetHeterogeneousArray+00014702 [ 14] 0x0000000015b78936 bin\win64\pgo\libmwlxeindexing.dll+00887094 MathWorks::lxe::assign_paren_shared_xvalue_ptr_uninitialized_to_struct+00006890 [ 15] 0x0000000015aac70f bin\win64\pgo\libmwlxeindexing.dll+00050959 MathWorks::lxe::at_rbrace_nargout+00006831 . ### Processing Template Makefile: C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\mbdtbx_s32k14x\mbdtbx_s32k14x\mbd_s32k14.tmf ### Creating sim_pil_target_AMMCLIB_s32k14x.mk from C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\mbdtbx_s32k14x\mbdtbx_s32k14x\mbd_s32k14.tmf ### Building sim_pil_target_AMMCLIB_s32k14x: .\sim_pil_target_AMMCLIB_s32k14x.bat C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\slprj\mbd_s32k14\sim_pil_target_AMMCLIB_s32k14x\instrumented>set MATLAB=C:\Program Files\MATLAB\R2018b C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\slprj\mbd_s32k14\sim_pil_target_AMMCLIB_s32k14x\instrumented>"C:\Program Files\MATLAB\R2018b\bin\win64\gmake" -f sim_pil_target_AMMCLIB_s32k14x.mk COPY_MDLREF_INCLUDES=0 GENERATE_ERT_S_FUNCTION=0 INCLUDE_MDL_TERMINATE_FCN=1 COMBINE_OUTPUT_UPDATE_FCNS=1 MULTI_INSTANCE_CODE=0 INTEGER_CODE=0 ISPROTECTINGMODEL=NOTPROTECTING Cleaning... RELATIVE_PATH_TO_ANCHOR is ..\..\..\.. ==== Removing object files from build directory ==== Copying necessary files to build directory... Compiler details : "C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\tools\gcc-6.3-arm32-eabi/bin/arm-none-eabi-gcc" -c -c -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O1 -g -gstrict-dwarf -DARM_MATH_CM4 -D__FPU_PRESENT=1 -D__FPU_USED=1 -D__NVIC_PRIO_BITS=FEATURE_NVIC_PRIO_BITS -o SetupFiles -DCPU_S32K144HFT0VLLT -I. -I.. -I..\..\..\.. -I"C:\Program Files\MATLAB\R2018b\simulink\include" -I"C:\Program Files\MATLAB\R2018b\extern\include" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src" -I"C:\Program Files\MATLAB\R2018b\rtw\c\libsrc" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src\ext_mode\common" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src\ext_mode\tcpip" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src\ext_mode\serial" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src\ext_mode\custom" -IC:\Users\YCHI~1\AppData\Roaming\MATHWO~1\MATLAB~1\TOOLBO~1\NXP_MB~1 -IC:\Users\YCHI~1\AppData\Roaming\MATHWO~1\MATLAB~1\TOOLBO~1\NXP_MB~1\slprj\mbd_s32k14\sim_pil_target_AMMCLIB_s32k14x -IC:\Users\YCHI~1\AppData\Roaming\MATHWO~1\MATLAB~1\TOOLBO~1\NXP_MB~1\S32_Examples\common\pil -IC:\PROGRA~1\MATLAB\R2018b\extern\include -IC:\PROGRA~1\MATLAB\R2018b\simulink\include -IC:\PROGRA~1\MATLAB\R2018b\rtw\c\src -IC:\PROGRA~1\MATLAB\R2018b\rtw\c\src\ext_mode\common -IC:\PROGRA~1\MATLAB\R2018b\rtw\c\ert -IC:\Users\YCHI~1\AppData\Roaming\MATHWO~1\MATLAB~1\TOOLBO~1\NXP_MB~1\slprj\mbd_s32k14\_sharedutils -I"C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\tools\gcc-6.3-arm32-eabi/arm-none-eabi/include" -I..\..\..\..\slprj\mbd_s32k14\_sharedutils -I"./common" -I"./inc" -I"./src/clock/S32K1xx" -I"./src/sim/S32K144" -I"./src/power/S32K1xx" -I"./S32K144/include" -I"../common" -I"../inc" -I"../src/clock/S32K1xx" -I"../src/sim/S32K144" -I"../src/power/S32K1xx" -I"../S32K144/include" Assembler details : "C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\tools\gcc-6.3-arm32-eabi/bin/arm-none-eabi-gcc" -c -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -g -x assembler-with-cpp -o SetupFiles Product: sim_pil_target_AMMCLIB_s32k14x_rtwlib.lib Build product type: library Building file ..\startup_S32K144.o... "C:\Users\y chi\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\tools\gcc-6.3-arm32-eabi/bin/arm-none-eabi-gcc" -c -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -g -x assembler-with-cpp -o ..\startup_S32K144.o ..\startup_S32K144.s gmake: *** [..\startup_S32K144.o] Error 1
### Build procedure for model: 'sim_pil_target_AMMCLIB_s32k14x' aborted due to an error.
Error(s) encountered while building "sim_pil_target_AMMCLIB_s32k14x"
I am just beginning to learn MBD and Embedded coder , So, I want to get some supports !  Thanks !
标签 (1)
0 项奖励
回复
2 回复数

3,011 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi [email protected]‌,

The actual release support only S32K14x derivaties.

The support the for the S32K11x (S32K116 and S32K118) is going to be released on July 22. Until that date you will not be able to use the PIL on S32K118.

Best regards,

Daniel

0 项奖励
回复

3,011 次查看
kunpeng_guo
Contributor I

ok ! thx for your answer!

kunpeng_guo

发件人: dumitru-daniel.popa

发送时间: 2019-06-18 20:53

收件人: kp g

主题: Re: - Re: PIL TEST【请注意,邮件由bounces+210748-d980-kunpeng_guo=ehawkeye.net@jiveon.jivesoftware.com代发】

NXP Community

Re: PIL TEST

reply from dumitru-daniel.popa in NXP Model-Based Design Tools - View the full discussion

Hi kp g,

The actual release support only S32K14x derivaties.

The support the for the S32K11x (S32K116 and S32K118) is going to be released on July 22. Until that date you will not be able to use the PIL on S32K118.

Best regards,

Daniel

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in NXP Model-Based Design Tools by email or at NXP Community

Following Re: PIL TEST in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 项奖励
回复