PIL SIMULATION and Build on board NXPs32k1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PIL SIMULATION and Build on board NXPs32k1

1,462 次查看
spinelli
Contributor I
 

Hello, I'm having an issue doing PIL simulation. I tried to fix following examples but i have problems even when i update i got an "Unable to update models referenced by 'test_model_3'. Caused by: Error(s) encountered while building "rtwshared" ". In one of the example the configuration for the board is set inside the referenced block in which i have my control logic. If i update the control logic opening it as top model i don't get any error. I checked for common issues like spacing o Configuration Parameter Setting; i propagated them to not have those problems. I installed some patches that fixed some problems but still not all of them. I see in the tree folder, in the _sharedutils_packaged the rtwshared.lib while in the _sharedutils the .mk and the .bat. Hope you can clear my ideas about this.

 

 
 
 
 
 
 

 

 
 
 
 
 
 

 

 
 
 
 
 
 

 

 
 
 
 
 
 

 

 
 
 
 
 
 
 
 
 
 
 
 
0 项奖励
回复
0 回复数