OpenCV for Microcontrollers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenCV for Microcontrollers?

2,473件の閲覧回数
matthiasroedder
Contributor III

Hey guys!

I'm using the K64f and I wanted to ask if there is any possibility to use OpenCV functions on it?

I've also heard of an alternative "OpenVx". Does someone has experience with this or other alternatives?

Thanks in advance!

Matthias

タグ(2)
3 返答(返信)

2,361件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected] ,

On this community we mainly handle questions regarding MATLAB/Simulink and our toolboxes. We currently do not have any support for openCV for the Kinetis family. I would suggest you ask on the Kinetis Microcontrollers community - there you should find help with this topic :smileyhappy:.

Kind regards,

Razvan.

2,361件の閲覧回数
matthiasroedder
Contributor III

Hello @Constantin Razvan Chivu,

okay thank you for the tip :smileyhappy:

Kind regards,

Matthias

2,361件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

[email protected] you are welcome! Hope you find all the answers you need there.

Kind regards,

Razvan.

0 件の賞賛
返信