OpenCV for Microcontrollers?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OpenCV for Microcontrollers?

2,484 次查看
matthiasroedder
Contributor III

Hey guys!

I'm using the K64f and I wanted to ask if there is any possibility to use OpenCV functions on it?

I've also heard of an alternative "OpenVx". Does someone has experience with this or other alternatives?

Thanks in advance!

Matthias

标记 (2)
3 回复数

2,372 次查看
constantinrazva
NXP Employee
NXP Employee

Hello [email protected] ,

On this community we mainly handle questions regarding MATLAB/Simulink and our toolboxes. We currently do not have any support for openCV for the Kinetis family. I would suggest you ask on the Kinetis Microcontrollers community - there you should find help with this topic :smileyhappy:.

Kind regards,

Razvan.

2,372 次查看
matthiasroedder
Contributor III

Hello @Constantin Razvan Chivu,

okay thank you for the tip :smileyhappy:

Kind regards,

Matthias

2,372 次查看
constantinrazva
NXP Employee
NXP Employee

[email protected] you are welcome! Hope you find all the answers you need there.

Kind regards,

Razvan.

0 项奖励
回复