Nxp S32k3xx supportPackage not loading hardware board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Nxp S32k3xx supportPackage not loading hardware board

跳至解决方案
2,104 次查看
avenkat
Contributor I

Trying to run a sample can project using the NXP s32k3xx using the official support package, but i keep on getting incorrect hardware board selected, and in the Configuraiton paramters, the nxp boards are available to to be select instead it takes me to "Get support Pakckages" and upon checking, i can confirm that the NXP support package for S32k3xx is installed, and the installation of NXP MDBT is verified and so is its license

0 项奖励
回复
1 解答
2,013 次查看
stefanvlad
NXP Employee
NXP Employee

Hello Avenkat,

 

I have a few questions about your software/hardware setup:

  1. What board are you using? 
  2. What Matlab version do you have? Can you show the Matlab Add-ons installed?

 

In order to have the best results you need to install the latest

  1. NXP_Support_Package​_S32K3xx version 1.4.0
  2. Model-Based Design Toolbox for S32K3xx version 1.4.0 

To the following location C:\MathWorks: 

stefanvlad_0-1708421001444.png

This should be the default location and you need to clean (delete) other folders like C:\Users\Your_User_Name\AppData\Roaming\MathWorks\MATLABAdd-Ons\Toolboxes\NXP_MBDToolbox_S32K3xx\ in order to have only one clean and good location, as in the picture above.

 

The following Add-ons need to be installed on your PC:

stefanvlad_1-1708421121027.png

 

Set the default path in Matlab, using the Set Path window --> Default --> Save --> Close:

stefanvlad_3-1708421812121.png

 

Then navigate to C:\MathWorks\Toolboxes\NXP_MBDToolbox_S32K3xx and run the path script file mbd_s32k3_path.m in the Matlab location:

stefanvlad_2-1708421722218.png

The output should be as in the picture above, with no errors.

 

Let me know how it works after you follow the steps above,

Stefan V.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,014 次查看
stefanvlad
NXP Employee
NXP Employee

Hello Avenkat,

 

I have a few questions about your software/hardware setup:

  1. What board are you using? 
  2. What Matlab version do you have? Can you show the Matlab Add-ons installed?

 

In order to have the best results you need to install the latest

  1. NXP_Support_Package​_S32K3xx version 1.4.0
  2. Model-Based Design Toolbox for S32K3xx version 1.4.0 

To the following location C:\MathWorks: 

stefanvlad_0-1708421001444.png

This should be the default location and you need to clean (delete) other folders like C:\Users\Your_User_Name\AppData\Roaming\MathWorks\MATLABAdd-Ons\Toolboxes\NXP_MBDToolbox_S32K3xx\ in order to have only one clean and good location, as in the picture above.

 

The following Add-ons need to be installed on your PC:

stefanvlad_1-1708421121027.png

 

Set the default path in Matlab, using the Set Path window --> Default --> Save --> Close:

stefanvlad_3-1708421812121.png

 

Then navigate to C:\MathWorks\Toolboxes\NXP_MBDToolbox_S32K3xx and run the path script file mbd_s32k3_path.m in the Matlab location:

stefanvlad_2-1708421722218.png

The output should be as in the picture above, with no errors.

 

Let me know how it works after you follow the steps above,

Stefan V.

0 项奖励
回复