No ERM ISR in eim_injection_s32k118 example project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No ERM ISR in eim_injection_s32k118 example project

2,390 次查看
dearwww2000
Contributor I

debug eim_injection_s32k118 example project, found no 'ERM_fault_IRQHandler()'. 

Why ?

It means that no need ?

What the user need to do with 'ERM_fault_IRQHandler()' ?

If no need, why we need to initialize the ERM module ?

What the ERM module give the user ?

标签 (1)
0 项奖励
回复
2 回复数

2,325 次查看
dearwww2000
Contributor I

'erm_report_s32k118' example project has ERM_ISR(), but only execute 'ERM_DRV_ClearEvent(INST_ERM1, 0U, ERM_EVENT_SINGLE_BIT);'.

What should we can do for ERM error ?

to Reset MCU ?

0 项奖励
回复

2,324 次查看
constantinrazva
NXP Employee
NXP Employee

Hello dearwww2000‌,

On this community we handle question regarding MATLAB/Simulink or our toolboxes. Unfortunately I can't help you on this topic, but I can suggest that you open a ticket for technical support here (go to 'Go to Ticket') or even better, ask this question on the https://community.nxp.com/community/s32/s32k  community.

 

Hope this helps,

Razvan.

0 项奖励
回复