Need information about S32k144 with MATLAB Embedder coder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need information about S32k144 with MATLAB Embedder coder

1,320件の閲覧回数
pratayay123
Contributor III

Dear Team,

Hope you are doing well. I need bellow information could please share those details.

1. Is the any tutorial /Workshop for S32K144- MATLAB/Simulink Modeling and embedder Code Generation.

2. Is there any working MATLAB model available for buck/ boost /buck boost converter with S32k144 and embedder coder.

3. is there any solution available for Battery Management system with S32k144.

 

Thanks,

Pratyay

0 件の賞賛
返信
1 返信

1,280件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @pratayay123 

Thank you for your interest into Model-Based Design Toolbox.

1. To learn more about MBDT capabilities for S32K144 I would recommend you the MBDT Beginner's Guide series of webinars, describing various features and functionalities of the toolbox - including how to develop applications that enable and use peripherals such as SPI, CAN, PWM, LIN, and Timers. This series of 7 webinars could be found on our MBDT Community webpage, in the right side of the screen.

Irina_Costachescu_0-1698913792724.pngIrina_Costachescu_0-1698913792724.png

2. We do not have at the moment an application targeting a buck boost converter delivered with MBDT for S32K1.

3. For Battery Management System on S32K144, please check the following webinar, where such a solution is presented: https://www.mathworks.com/videos/deploying-battery-management-system-algorithms-on-nxp-s32k-from-sim...

For more details and information on MBDT for S32K1, you could also check the Webinars section (placed under MBDT Beginner's Guide series), where you could find videos targeting topics such as motor control applications, how to verify and validate algorithms inside the Simulink ecosystem, and others.

Please let us know if you encounter any issues/questions while using MBDT.

Thank you,

Irina

 

0 件の賞賛
返信