Need help with MBDT and MPC5748G target for ADC configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help with MBDT and MPC5748G target for ADC configuration

1,361件の閲覧回数
zcampbell
Contributor I

I have been trying the follow along with the video series for BLDC Motor Control with MBDT Training course and the devkit I had purchased from NXP was not of the same type as the training course.  So, I have been following the examples along until I need to change PN of my application.  In starting with the ADC programming tutorial number 4, I changed the Target type to my target board (an MPC5748G).  When I do this, the ADC config and the ADC start blocks appear to say that ADC is unsupported by the MCU.  This does not seem to be correct.  This is also happening when I launch Simulink examples and switch the Target to my MPC5748G.  Based on manual excerpt, I have quite a bit of ADC available to me...  Please help...

pastedImage_1.png

0 件の賞賛
返信
1 返信

1,277件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello zcampbell@amshowa.com‌,

Unfortunately the message is right. The MBDT toolbox does not currently support the ADC conversions on MPC5748G. The MPC5744P is more suitable for motor control applications.

Hope this helps,

Marius

0 件の賞賛
返信