NXP_s32k3xx_toolbox_installation_problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP_s32k3xx_toolbox_installation_problem

1,342件の閲覧回数
Mahesh12
Contributor I

Hi, Recently I was installing S32K3 MATLAB toolbox , at first there is pop up with Installation failure  when I click on Add as "Community authored toolbox are temporarily unavailable" and then tried with downloading .mtblx file in MATLAB file exchange 

 

image (1).png

 

Next downloaded file from NXP website  but again during installation of.mtblx file as Add on , there is pop up as"Toolbox cannot be installed because it is not a valid toolbox"            please help me in installing this 

image.png

0 件の賞賛
返信
1 返信

1,311件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hello @Mahesh12 

If the MathWorks Add-Ons installation is not working as expected, please note that there is also another way in which you can install MBDT toolboxes.

Can you please follow the steps described in this thread (link), with the only change that the MBDT for S32K3 will be the toolbox that you will need to access?

MBDT for S32K3 v1.5.0 (the latest available) can be found at the following location: link: https://nxp.flexnetoperations.com/control/frse/download?element=3983098

Please let us know if this installation method works on your setup or if further guidance is required from our side.

Thank you,

Irina

0 件の賞賛
返信